Configuration function calls
The following table provides a brief description and a link to each API function.
API function | Description |
Adds a data item to the data definition table. | |
Returns the number of data definitions that can still be added to the data definition table. | |
Initializes the data definition table. | |
Initializes the data definition table and enables optional DTL features. | |
Returns the number of bytes needed to store data in application data type format. | |
Returns the application data type from a data definition. | |
Uninitializes the data definition table. |
Provide Feedback