Format of the piunsol.ini file
Piunsol.ini consists of a series of entries, one for each 5820-EI module RSLinx Classic will register with for unsolicited messages. For example:
[130.151.188.135]
0200=4
010070=16
where
[130.151.188.135]
is the hostname or dot address of the 5820-EI0200
is the first PLC-2 memory address to register4
is the length of that memory address010070
is the second PLC-2 memory address to register16
is the length of that memory addressAddress is expressed in octal and length is expressed in decimal. The examples show the common leading 0 just for convenience. Notice that the same PLC-2 memory address/length pair can appear in multiple hostname entries.
Provide Feedback