Unsolicited message function calls

The following table provides a brief description and a link to each API function.
API function
Description
Changes a PCCC command packet into a reply packet.
Sends the unsolicited reply to the originator.
Registers a client application for broadcast style unsolicited messages.
Unregisters a client application for broadcast style unsolicited messages.
Registers a client application for PLC-2 style unsolicited messages.
Unregisters a client application for PLC-2 style unsolicited messages.
Registers for unsolicited messages from a specific target station.
Unregisters for unsolicited messages from a specific target station.
Registers a client application for virtual-link style unsolicited messages.
Unregisters a client application for virtual-link style unsolicited messages.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal