DTL_UNSOL_SOURCE_REGISTER

The DTL_UNSOL_SOURCE_REGISTER function registers for unsolicited messages from a specific target station. If successful, all messages from the station specified by
dtsa
are delivered to
pfCallback
, with the
dwCallbacK
passed along for the caller's convenience. An application can have multiple simultaneous targets registered. No other application will receive any messages from the registered station.
DTL_RETVAL LIBMEM DTL_UNSOL_SOURCE_REGISTER(
handle,
dtsa
,
pfCallback
,
dwCallback
,
dwTimeout
)
DWORD*
handle
;
/* pointer to handle library will set
DTSA_TYPE*
dtsa
;
/* DTSA pointing to source of messages
DTL_UNSOL_CALLBACK
pfCallback
;
/* pointer to function
DWORD
dwCallback
;
/* callback identifier
DWORD
dwTimeout
;
/* timeout value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal