Use the software with Ethernet modules
If you selected Ethernet as the module type when you opened or created the current configuration, you can configure a Rockwell Automation Ethernet communication module (1756-ENB, 1756-ENBT, 1756-EWEB, 1756-EN2T/R, 1756-EN2F, 1783-ETAPxx) using the ControlLogix Gateway configuration tool. You can create and save configuration files associated with the Ethernet module to a disk.
Provide Feedback