Configure an Ethernet/IP port with auto port speed
To configure an Ethernet communication port, perform the following steps:
- In theNetwork Configuration Typegroup box, specify the network type (Dynamic or Static).TIP: If you select aDynamic network type, you can perform step 2, and then steps 10 through 13 only. If you select aStatic network type, you can perform steps 3 through 13.
- Select one of the two interface configuration values (BOOTP or DHCP), determining the method that the device will use to obtain an initial IP address at start-up.TIP: If the address is accessed through a Network Address Translation (NAT) device, a warning message shows on thePort Configurationtab. Input the private IP address in theIP Addressbox. If you change the private IP address, you must change the NAT device configuration accordingly.
- Specify the IP Address of the device.
- Specify theNetwork Mask(or subnet mask) of the device.
- Specify a defaultGateway Address, indicating the IP address of the default gateway of the device.
- Specify the address of thePrimary Name Server(or DNS server). This address is used to resolve host names.
- Specify the address of theSecondary Name Server(or DNS server). This address is used when the primary name server is not available or unable to resolve a host name.
- Enter aDomain Name(maximum of 48 characters). This name is used when resolving host names that are not fully qualified.
- Enter aHost Name(maximum of 64 characters).
- If you want to read the port speed and duplex values automatically from the device (these values cannot be edited), select theAuto Negotiatecheck box. If you want to edit the port speed and duplex values, clear theAuto Negotiatecheck box and perform the following steps:
- Select the Current Port Speed (10, 100, or 1000 Mbps).
- Select the Current Duplex configuration mode (Half or Full).
- ClickApplyto download changes to the module.TIP: If you chose to manually select the post speed and duplex mode, and you clickApply, the network communication will be briefly interrupted. For some devices, you must enter a password to save the changes if the device is configured to require a password.
- Review theStatusfield for information about the communication port (Network Interface Configured,Network Interface Not Configured).
- ClickOKto complete the configuration.
Provide Feedback