Configure an Ethernet port when using a Bootp server
To configure an Ethernet port, you have an option of using the Rockwell Software Bootp Server utility, which is shipped with RSLinx Classic. To access this utility, click
Start > Programs > Rockwell Software > BOOTP-DHCP Server > BOOTP-DHCP Server
. For further information on how to use the utility, from the BOOT-DHCP Server's
main menu, select View > Help
.Provide Feedback