View general information about your module
When you open or create the current configuration, select the
General
tab to view
the general information about the module. The General
tab provides the following
information about your ControlNet, DeviceNet, EtherNet, 1756-DH485, or 1756-DHRIO
module:- Device name
- Vendor name
- Product type
- Product code
- Revision level of the firmware within the device
- Serial number
- Faults
Provide Feedback