Site-Level Dashboard

Offers detailed energy consumption and efficiency metrics for individual sites. This level helps site managers monitor and optimize energy usage, identify inefficiencies, and implement site-specific energy-saving measures.
Click
Site
from the hierarchy list. The site dashboard consists of
Overview
and
Distribution
tabs.
Overview
Under the
Overview
tab, the user can view charts of energy consumption and emissions of all electrical and non-electrical energy types based on the time period selected from the date picker.
Site-level Dashboard
The application displays consumption and demand data for all resource and utility types rolled up from the meter level to the node and site levels. These widgets and charts are organized alphabetically, and enable users to observe demand patterns and consumption across the hierarchy. These widgets are rendered dynamically based on what is configured and mapped in the system automatically when meters are added or removed.
NOTE:
The utilities and non-energy type resources will not be a part of the Energy, Cost and Emission calculations.
The following table provides a list of charts available by default in the Site-level dashboard under
Overview
tab:
Chart Types
S.No
Chart/Widget Name
Description
1
Resources (Donut Charts)
Energy
: This is the overall summary of the total energy consumption, with the values of each resource type along with default units.
Cost
: This is the overall summary of the total cost with the values of each resource type.
Emission
: This is the overall summary of the resource emission, with the values of each resource type.
The table displays the top 3 resource types.
A list of resource types is displayed on clicking the expand icon on the top left corner of the widget.
In the expanded view, all the records are listed.
2
Energy Consumption by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and consumption on the Y-axis. This chart shows the overall energy consumption summary with default values (hover the mouse and you see the data with default values).
3
Costs by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and cost on the Y-axis. This chart shows the overall energy cost summary.
4
Emissions by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and emissions on the Y-axis. This chart shows the overall emission summary.
5
Energy Intensity
The user can view the selected time period with the respective granularity on the X-axis and energy intensity on the primary Y-axis, production data on the secondary Y-axis. This chart shows the overall energy intensity summary with the comparison of production data.
6
Production Data
The user can view the selected time period with the respective granularity on the X-axis and production data on the Y-axis. This chart shows the overall production summary.
7
Total Consumption - Production Chart
The user can view the selected time period with the respective granularity on the X-axis and consumption in the primary Y-axis, and production data in the secondary Y-axis. This chart shows the overall consumption summary with the comparison of production data.
8
Resource / Utility Consumption Data
The user can view the consumption of the configured resource/utility of the selected time scope with the respective granularity on the X-axis and consumption details on the Y-axis.
9
Resource / Utility Demand Data
The user can view the demand of the configured resource/utility of the selected time scope with the respective granularity on the X-axis and demand details on the Y-axis.
10
Energy Consumption (Heat Map)
The X-axis and Y-axis granularity values are represented based on your time period selection. This chart shows the overall consumption summary in the heat map format with color representation.
Refer to Dashboard Features section to manage the Site-Level dashboard.

Distribution

Under the
Distribution
tab,
Resource Distribution
chart is displayed. This displays the Resource distribution (Sankey Diagram) from
Site
to
Area
to
Work Center
.
User can change the resource type from the Resource Type dropdown and visualize the resource distribution for configured Resource types.
Site-Level Distribution Dashboard
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal