Add Area Node

The Area Level dashboard provides insights into energy usage within specific areas of a site. It helps area managers track energy performance, identify high-consumption zones, and implement localized energy-saving initiatives.
NOTE:
The following points are required to view data on
Area level dashboard
:
  • Data from different meters which are a direct child of the Area node will be considered for data aggregation.
  • To show the data of all the available charts, the respective resource meter to be configured with the correct tag mapping.
  • For Cost charts, the respective rate schedule should be configured at the Site level.
  • For Emission, the respective emission factor should be configured at the Site level.
  • For Production, energy intensity charts should have correct tag mapping for production count measurement.
  • For more than one resource meter harmonized unit defined at the Enterprise level will be used for displaying data for consumption, intensity, and emission.
Perform the following steps to add an Area under a Site:
  1. Select
    Site
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    Site - Add
    The
    Add Component
    dialog is displayed.
    Add Component
    User can also add the Area from the Site Configuration page.
    Add Area from Site
  3. Under
    Node
    , select
    Area
    and provide the following details:
    • Name
      : Provide an area name.
    • Description
      : Provide a description of the Area.
    Add Component Dialog
  4. Click
    Add
    .
    The "
    Added successfully
    " message is displayed.
  5. To edit the base details and set the notification, refer to the Edit Component and Notification Configuration sections.
    Area
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal