Remove Component
Perform the following steps to remove the component from the hierarchy list:
- Select the required component.
- Click the [
] icon and click
Remove. - In theRemove Hierarchy Componentdialog box, clickRemove.Remove Hierarchy Component Dialog

The "
Deleted successfully
" message is displayed.
NOTE:
The user cannot remove the parent component directly. The user needs to remove the child component first and then the user can remove the parent component from the hierarchy list.
If the user removes the parent component directly, the following notification message is displayed:
Remove Hierarchy Component

Provide Feedback