Add Work Center Node
The Work Center Level dashboard focuses on energy consumption and efficiency within specific work centers. This level allows for detailed monitoring of energy usage in production or operational units, helping managers optimize processes and reduce energy waste.
NOTE:
The following points are required to view data on
Work Center level dashboard
:- Data from different meters which are directly connected to a Work Center node will be considered for the data aggregation.
- For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
- For Cost charts, the respective rate schedule should be configured at the Site level.
- For Emission, the respective emission factor should be configured at the Site level.
- For Production and energy intensity charts should have correct tag mapping for production count measurement.
- Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add a Work Center under an Area:
- SelectAreafrom the hierarchy list.
- Click the [
] icon and click
Add.Area - Add
TheAdd Componentdialog is displayed.Add Component
- UnderNodefrom the left pane, selectWork Center.Add Component- Work Center Dialog

- Provide the following details:
- Type: Select aWork Centertype from the dropdown list.Work Center Types

- Name: Provide a Work Center name.
- Description: Provide a description of the Work Center.
- ClickAdd.The "Added successfully" message is displayed.
- To edit the base details and set the notification, refer to the Edit Component and Notification Configuration sections.Work Center

Related Information
:Provide Feedback