Add Work Unit Node
Offers granular insights into energy usage at the work-unit level. It enables precise tracking of energy consumption for individual machines or processes, facilitating targeted energy-saving actions and maintenance planning.
NOTE:
The following points are required to view data on
Work Unit level dashboard
:- Data from different meters which are directly connected to a Work Unit node will be considered for the data aggregation.
- For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
- For Cost charts, the respective rate schedule should be configured at the Site level.
- For Emission, the respective emission factor should be configured at the Site level.
- For Production and energy intensity charts should have correct tag mapping for production count measurement.
- Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add Work Unit:
- Select aWork Centerfrom the hierarchy list.
- Click the [
] icon and click
Add.Work Center - Add
TheAdd Componentdialog is displayed.Add Component
- UnderNodefrom the left pane, selectWork Unit.Add Component - Work Unit Dialog

- Provide the following details:
- Type: Select a Work Unit type from the dropdown list.Work Units Types

- Name: Provide a Work unit name.
- Description: Provide a description of the Work Unit.
- ClickAdd.The "Added successfully" message is displayed.
- To edit the base details and set the notification, refer to the Edit Component and Notification Configuration sections.Work Unit

Related Information
:Provide Feedback