Configure Rate Schedules

This feature allows users to manage and adjust the cost associated with different resources over specific timeframes. This feature enables the systematic setup and modification, which can be based on time periods and resource types.
Add Rate Schedules
Perform the following steps to add a rate schedule:
  1. Under the
    Rate Schedules
    tab, click
    Add
    .
  2. In the
    Add Rate Schedule
    dialog box, set these parameters:
    • Resource/Utility Type
      : Select a resource/utility type from the dropdown list.
    • Valid From
      : Click the [] icon and select the date.
    • Vendor Name
      : (Optional) Provide a name.
    • Time
      : Select a rate schedule period by using the angular-slider.
    • Resource Rate
      : Provide a resource rate value.
  3. Click
    Add
    .
    Add Rate Schedule
    The "
    Added successfully
    ” message is displayed. User can add multiple Rate Schedules and they are displayed under each resource/utility type dropdown.
Edit Rate Schedule
Perform the following steps to edit the rate schedule:
  1. Under the
    Rate Schedules
    tab, the user can view the list of all available resource/utility types.
  2. On the required resource type, click the [] icon.
    Rate Schedules
    User can hover over a rate schedule to view the details, as shown below:
    Rate Schedule Details
  3. In the
    Edit Rate Schedule
    dialog box, edit the fields and click
    Save
    .
    Edit Rate Schedule
    The "
    Updated successfully
    ” message is displayed.
Delete Rate Schedules
NOTE:
A user can delete a Rate Schedules only when multiple Rate Schedules are available for the selected resource/utility type.
Perform the following steps to delete the rate schedule:
  1. On the required resource/utility type, click the [] icon.
  2. In the
    Delete Rate Schedule
    dialog box, click
    Delete
    .
    Delete Rate Schedule
    The “
    Deleted successfully
    ” message is displayed.
NOTE:
If there is an overlap in the rate schedule time period, no notification is shown; however, the time periods will align automatically upon saving.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal