Dashboard Features
These dashboard features allow users to manage the charts/widgets and view the details at a given data point.
Dashboard - Enterprise/Region

Dashboard Features Site/Area/Work Center/Work Units

These features are explained in the following sections:
Provide Feedback