Create a key button

At runtime the operator can use key buttons to move the cursor and make selections on certain objects. You can use key buttons with control list selectors and display list selectors.
FactoryTalk View
supports multiple type of key buttons. You can configure any combination of key buttons in a display containing a list object or trend. Add and configure each key button separately.
TIP:
You can set up auto repeat for four of the key buttons:
Move Up
,
Move Down
,
Page Up
, and
Page Down
. Set up auto repeat in the
Timing
tab.
To create a key button:
  1. In the
    Graphics
    editor, click
    Objects > Key
    and enter a name for the key button. You can also click
    Key
    in the
    Toolbox
    .
  2. Drag the mouse into position and draw a rectangle.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal