Key Button Properties - Timing tab

The following table shows the options of the
Timing
tab of
Key Button
Properties.
Options
Description
Auto repeat rate
Select the number of times per second a button press is registered when the button goes into auto repeat mode. Select 0 if auto repeat is not to be used.
Auto repeat delay
Select the length of time the button has to be pressed and held down before auto repeat starts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal