Set up auto repeat for a key button
If you set up auto repeat, when the operator presses and holds down the key button, repeated button presses are registered until the operator releases the button. You can set up auto repeat for the Move Up, Move Down, Move Left, Move Right, Page Up, and Page Down key buttons.
To set up auto repeat for a key button:
- In a display, double-click the key button to open itsPropertiesdialog box.
- Click theTimingtab.
- Specify the auto repeat settings to use with the key button.
Provide Feedback