How the key button works at runtime

The key button’s behavior at runtime depends on which other objects appear on the display with it, and whether the key button's
Send press to
property is set to
Object With Focus
or
Linked Object
.
Key buttons do not work with all objects. If a key button's
Send press to
property is set to
Object With Focus
, but the object with focus on the display does not work with the key button, when the operator presses a key button, nothing happens. Also, if a key button whose
Send press to
property is set to
Object With Focus
, is pressed when no object has focus, nothing will happen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal