Configure general properties of a key button

Once you set up the options in the
General
tab, click the
Label
tab to specify a caption or image for the key button.
To configure general properties of a key button:
  • In the key button
    Properties
    dialog box, in the
    General
    tab, specify the following properties if needed:
    • general appearance
    • touch margins
    • audio (whether the key button beeps at runtime)
    • whether the button press will be sent to whatever object has input focus or to a specific object linked to the button
      TIP:
      If you choose to send the button press to a linked object, click on the browse button (...) in the Linked object field to open the Object Browser and select the object to link to.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal