Standard I/O Modules

Rockwell Automation offers many I/O modules for use in
ControlLogix®
controller systems. When you select I/O modules, remember the following:
  • A wide variety of digital, analog, and specialty I/O modules support the following features:
    • Field-side diagnostics
    • Electronic fusing
    • Individually isolated inputs/outputs
    • Timestamping of inputs
    • Scheduling of outputs
    • Event detection of specific input patterns
  • Removable terminal blocks (RTBs) or 1492 wiring systems are required for I/O modules.
  • 1492
    PanelConnect
    modules and cables can be used to connect input modules to sensors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal