Add Remote I/O to the Ethernet Port on the Controller

If you are adding remote I/O modules, you can add the I/O modules to an Ethernet port of the controller. Typically, you must add a remote
EtherNet/IP
communication module before you can add the remote I/O modules.
To add a remote
EtherNet/IP
communication module to your project, complete these steps.
IMPORTANT:
You cannot bridge through the front Ethernet port of another controller to add remote I/O.
  1. In the I/O configuration, right-click Ethernet and select New Module.
    This image shows how to add a remote I/O module in the I/O Configuration of Logix Designer.
  2. On the Select Module Type dialog box, select the remote
    EtherNet/IP
    device and, click Create.
    TIP:
    Use the filters to reduce the list of modules to choose from.
    This image shows how to select an EtherNet/IP module in Logix Designer.
    TIP:
    For some modules, the Select Major Revision dialog box can appear. If the dialog box appears, choose the major revision of the module and click OK.
    If the Series and Revision parameter values do not match those of the module for which this configuration is intended, your project can experience module faults.
  3. Configure the remote
    EtherNet/IP
    communication module according to your network configuration, and click OK.
    This image shows where to click OK in Logix Designer after configuring an EtherNet/IP module.
  4. At the warning dialog box, click Yes and then close the Select Module Type dialog box.
    IMPORTANT:
    If you inhibit the module connection, you must remember to uninhibit the connection later.
    This image shows the warning before you can create a new module online in Logix Designer.
  5. Close the Select Module Type dialog box.
  6. Right-click the backplane of the newly added
    EtherNet/IP
    communication module and select New Module.
    This image shows how to add a new remote I/O module in Logix Designer.
  7. On the Select Module Type dialog box, select the I/O module and click Create.
    This image shows how to select and create a remote I/O module in Logix Designer.
  8. Configure the I/O module, and click OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal