Add Local I/O Modules

While your controller project is offline, use the New Module option to add I/O modules to add them to the project. To add modules while the project is offline, complete the following steps.
  1. In the I/O configuration, right-click the backplane and select New Module.
  2. On the Select Module Type dialog box, select the I/O module and click Create.
    TIP:
    Use the filters to reduce the list of modules to choose from.
    This image shows how to create a new 1756 I/O module in Logix Designer.
  3. On the New Module dialog box, configure the module and click OK.
    This image show the New Module dialog box in Logix Designer.
    TIP:
    If the series or revision values in the module properties do not match those of the module for which this configuration is intended, your project can experience module faults.
    This image shows where the 1756 I/O module series and revision are in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal