Remote I/O Modules
Remote I/O refers to I/O modules that are not in the local chassis and connect to the controller via a communication network. There are several families of I/O modules that are remote from the controller:
- I/O modules in a remote chassis via a network bridge module
- Distributed I/O families
- On-Machine™I/O families
The
ControlLogix®
controller supports the use of remote I/O via these networks:- EtherNet/IP™
- DeviceNet®
- Universal remote I/O
For more information about the network configurations that can be used to connect remote I/O, see Communication Networks.
ControlLogix 5580 Controller and Remote I/O on a 1 Gbps EtherNet/IP Network
Provide Feedback