System Banner
The
System Banner
appears at the top of each screen in a project by default. It contains default navigation items:- A button to open theAlarmSummaryscreen
- The current number of unacknowledged alarms
- PreviousandNextbutton
- The username of the logged on user.
- Diagnostic icons indicating the status of data logging and project events.
- Network and controller status
- The current date and time for the HMI device
- Controller information for controller issues
The HMI designer may change the
System Banner
to: - Add graphic elements, such as buttons, text displays, or configured elements such as a gauge to display a data value.
- Omit default items.
- Change the appearance of theSystem Banner, such as background color or height.
Graphic elements with invalid tag values are outlined in red on the HMI device. An
pointing down appears in the
Error
icon System Banner
for graphic elements with invalid tag values that exist outside of the System Banner
.Provide Feedback