Navigation menu
Use the
Navigation menu
to browse the contents of the application and open screens. The Navigation menu
on the HMI device displays the contents of the project in Studio 5000
View Designer
. The Navigation menu
appears at the bottom or left side of the HMI device screen. To access the Navigation menu
- SelectNavigationin theSystem Banner
- Push the button on the HMI device.
- PressAlt+Non an external keyboard.
The menu items in the
Navigation menu
depend on the security access granted to the security role assigned to the logged on user. Security is set in Studio 5000
View Designer
. For the Operator role, the Navigation menu
displays only the items to which the Operator has access. Guest is the default user. When not logged in, only the items to which the Guest role has access appear in the Navigation menu
. Provide Feedback