System Banner contents
By default, a
System Banner
with default content appears at the top of each screen. The HMI designer may configure the System Banner
to add or remove items from the System Banner
. 
Item | Description | |
![]() | Alarm Status Indicator opens the Alarm Summary screen on the HMI device.
| |
![]() | ![]() | Automatic Diagnostics Indicator opens Automatic Diagnostics screen on the HMI device. The button shows a notification with the number of active diagnostics. The button returns to an outlined icon when no diagnostics are active. |
![]() | Previous displays the previous screen in the navigation history on the HMI device. | |
![]() | Next displays the next screen in the navigation history on the HMI device. To navigate with Next requires displaying a previous screen first. | |
![]() | ![]() | Navigation displays the Navigation menu at the bottom of the screen on the HMI device. Use the Navigation menu to display shortcuts and folder contents. |
![]() | Log On logs on or off the project. The name of the logged on user appears in the System Banner . The logged on user sees only the screens for which the assigned user role has access. | |
![]() | General Diagnostics Status for the data log status and project event
errors. These icons appear depending on the status of data export and project
events.
A data log status icon only appears when a project contains a data log and there
are no project event errors.
| |
![]() | A Network Status icon appears only if there is an issue with network communication. Select the icon to open the HMI Device Configuration Network popup for details about the issue.
| |
![]() | A Controller Status icon appears only if there is an issue with any controller in the project. Select the icon to open the Controllers General popup for details about the issue.
| |
![]() | The current time and date of the HMI device. | |
Provide Feedback

The button on the screen turns red and flashes when there are active alarms that are unacknowledged.
The button returns to a gray icon with a numbered notification showing the number of unacknowledged alarms when all alarms return to normal but some alarms are still unacknowledged.
The button turns to red when there are active alarms and all of them are acknowledged.