Virtual Standard Keyboard
The
Virtual Standard Keyboard
opens when interacting with a graphic element that requires text input. 
Item | Description |
![]() | Type characters in the Input box. Any entry for the graphic element appears highlighted automatically when the Virtual Standard Keyboard opens. There is no limit to the number of characters in the Input box. The characters at either end of the Input box appear with a gradient when not all of the typed characters are visible. Scroll horizontally to see the remaining characters. |
![]() | Clear removes all characters from the Input box. This key appears only when there are characters in the Input box. |
![]() | Backspace deletes one character to the left at a time. |
![]() | Language Selector displays an alpha European character on each key. Display characters in upper or lowercase. |
![]() | Symbols displays a symbol on each key. To re-display the standard alpha characters, tap ABC ,Symbols . |
![]() | Shift toggles the keyboard between uppercase and lowercase letters for one keystroke. |
![]() | Caps Lock toggles the between uppercase and lowercase letters. The Virtual Standard Keyboard remains in the selected state until you tap Caps Lock again. |
Provide Feedback


removes all characters from the 
deletes one character to the left at a time. 
displays an alpha European character on each key. Display characters in upper or lowercase. 
displays a symbol on each key. To re-display the standard alpha characters, tap
.
toggles the keyboard between uppercase and lowercase letters for one keystroke.