FactoryTalk ViewPoint Help

FactoryTalk®
ViewPoint is an add-on to
FactoryTalk View
that serves fully animated, read and write displays of
FactoryTalk View
applications to a web browser. Published displays are accessible on demand, with no additional
Rockwell Automation
software required.
FactoryTalk ViewPoint for Machine Edition
applications are uploaded to and served from a
PanelView™
Plus operator terminal. When connected to the
FactoryTalk ViewPoint
server's network, open a browser on your desktop or mobile device, enter the hostname or IP address of the
PanelView Plus
graphic terminal, and view live information about your plant or process.
Rockwell Automation
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal