Disconnect from a web application
Disconnect from a web application to stop viewing displays and free the
FactoryTalk ViewPoint
license for another user.To disconnect from a web application
Use one of these methods:
- Close the browser.FactoryTalk ViewPointreleases the license within 30 seconds.
- On the desktop banner, click
or the username. FactoryTalk ViewPointreleases the license immediately.
Provide Feedback