Navigate displays

Each display presents different information about your plant or process, as designed in
FactoryTalk View Studio
. Navigate between displays to change the information presented in the web browser.
The buttons, touch animations, and macros used to navigate displays vary by application, as designed in
FactoryTalk View Studio
. Bookmark or favorite individual display URLs to load the display without using the navigation provided by the application.
To navigate between displays
  • Use a button, touch animation, or macro designed in the application.
  • Use the browser's forward, back, favorites, and history features to save and load displays by URL.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal