Analyze data in FactoryTalk ViewPoint trends
A FactoryTalk ViewPoint trend displays real-time pen values from a data server defined in a
FactoryTalk View
trend object. A FactoryTalk ViewPoint
trend will not display any pen values if the corresponding HMI servers, data servers, or FactoryTalk View ME
applications are unavailable or not running.Most features of a
FactoryTalk ViewPoint
trend cannot be modified in a web browser at runtime. To change pen definitions or properties, open FactoryTalk View Studio
, modify the original object, and then publish the changes to the web application.FactoryTalk ViewPoint
trends do not support:- Historical data fromFactoryTalk View MEdata log models
- Trend overlays
- Trend templates
Provide Feedback