Pan a trend

Zoom a trend to increase or decrease the amount of time shown in a trend chart. The trend stops scrolling when zoomed, but the slider continues to move as the trend retrieves data from the server.
To zoom a trend chart
  1. Select the left or right slider handle.
  2. Drag the slider handles closer together to zoom out or further apart to zoom in.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal