Change tag values at runtime

If the signed in user has write permissions to a display, objects on the display can change tag values at runtime. When the tag value is changed, a status message indicates whether the tag write completed successfully. If the tag write does not complete successfully, an error message is shown.
TIP:
The status bar appears at the bottom of the display as a default. Click the "x" to close the status bar.
Tag values can be changed using the following graphic objects:
Push buttons and control list selectors behave identically to their
FactoryTalk View
counterparts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal