Change display scaling

Graphic displays are automatically resized and scaled to fit the web browser window, regardless of settings specified for the display in
FactoryTalk View Studio
. When displays are scaled, the original aspect ratio is not preserved.
Pop-up displays are always sized in proportion to the displays from which they were opened. Docked displays that allow resizing are scaled in proportion to the web browser window. Undocked displays opened alongside docked displays will scale to fit the available client area.
To preserve the display aspect ratio
  • In the web browser's
    Address
    bar, add
    &RetainAspectRatio=True
    to the display URL, and then press
    Enter
    .
To disable display scaling
  • In the web browser's
    Address
    bar, add
    &ScaleToScreen=False
    to the display URL, and then press
    Enter
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal