Upgrade firmware using an upgrade card
If you want to upgrade a terminal from an external storage card, use the Firmware Upgrade Wizard to create a firmware upgrade card that can be plugged into the terminal to perform a firmware upgrade.
To upgrade firmware using an upgrade card
- Plug a blank Secure Digital (SD) card into your computer.
- Open the Firmware Upgrade Wizard.Use one of the following methods:
- From WindowsStartmenu, selectAll apps > Rockwell Software > ME Firmware Upgrade Wizard.
- InFactoryTalk View Studio, from theToolsmenu, selectFirmware Upgrade Wizard.
- Select the KEPServer drivers, if any.
- Plug this upgrade card into the terminal's card reader.
- Press theUpgradebutton.
The terminal is automatically restarted.
When upgrading the firmware on a
PanelView Plus 7
or PanelView Plus 6
terminal, do not remove the card until you see the following message: "The firmware upgrade has been completed. Remove the Firmware Upgrade Card and then press the Exit
button." Premature removal of the card will cause the upgrade to fail.Provide Feedback