Select a KEPServer

If your application use one or more KEPServer OPC servers, you can include KEPServer drivers in your firmware upgrade. By default, no drivers are selected when the Firmware Upgrade Wizard is first used. If a selection has been made in a previous upgrade, that selection will be selected.
TIP:
The Kepware Hilscher Universal communications driver is only supported for the following terminals:
  • PanelView Plus 6
    700-1500
  • PanelView Plus 6 Compact
    1000
To select a KEPServer driver
  1. Select the box beside the name of each driver that you want to include in your firmware.
  2. Click
    Next
    .
The next step presents a summary of your selections and finishes the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal