Upgrade firmware from a remote computer
When the terminal is connected to a
Windows
computer running the Firmware Upgrade Wizard, you can perform a remote upgrade.To perform a remote upgrade
- Open the Firmware Upgrade Wizard.Use one of the following methods:
- From WindowsStartmenu, selectAll apps > Rockwell Software > ME Firmware Upgrade Wizard.
- InFactoryTalk View Studio, from theToolsmenu, selectFirmware Upgrade Wizard.
- Select the terminal in theCommunicationstree.
- Select the KEPServer drivers, if any.
The terminal is automatically restarted by the Wizard.
Provide Feedback