About the Firmware Upgrade Wizard

How do I open the Firmware Upgrade Wizard?
Use one of the following methods:
  • From Windows
    Start
    menu, select
    All apps > Rockwell Software > ME Firmware Upgrade Wizard
    .
  • In
    FactoryTalk View Studio
    , from the
    Tools
    menu, select
    Firmware Upgrade Wizard
    .
As
FactoryTalk®
View Studio evolves over time, new versions of terminal firmware become available. Once you have acquired a new firmware release, use the Firmware Upgrade Wizard to replace the firmware files on your ME terminals.
The Firmware Upgrade Wizard allows you to upgrade the firmware in a
PanelView™
Plus 7 Performance Series A,
PanelView Plus 7 Standard
, or
PanelView Plus 6
terminal from a remote computer, or to put the firmware upgrade onto an external storage card that can be plugged directly into the terminal to complete the upgrade. If you do not have a card available, you can copy the firmware upgrade to a specified location on your computer and transfer them to a card manually later.
  • To upgrade from a remote computer, the terminal must be connected to a
    Windows
    computer running the Firmware Upgrade Wizard. The connection can be a network connection using
    FactoryTalk® Linx
    , or, if the
    FactoryTalk Linx
    services are not available, a direct Ethernet or serial connection.
    IMPORTANT:
    For remote upgrades, the Firmware Upgrade Wizard requires that the Remote Access Connection Manager be installed and running on the computer running the Firmware Upgrade Wizard. See your Microsoft Windows help for more information on how to set it up.
  • To upgrade from an external storage card, use the Firmware Upgrade Wizard to create a firmware upgrade card that can be plugged into a terminal to perform a firmware upgrade.
    TIP:
    • To upgrade firmware on a
      PanelView Plus 7 Performance
      Series B terminal, use
      ControlFLASH™
      or
      ControlFLASH Plus®
      . For more details, see
      PanelView Plus 7 Performance
      Series B Quick Start Guide
      , publication 2711P-QS002.
    • To upgrade firmware on a
      PanelView Plus
      ,
      PanelView Plus Compact
      , or
      PanelView Plus CE
      terminal, use
      FactoryTalk View
      v12.00.00 or earlier.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal