What is firmware?

Each firmware release contains:
  • FactoryTalk Services Platform
  • FactoryTalk View ME Station
  • FactoryTalk ViewPoint
  • KEPServer (optional)
  • FactoryTalk Linx
  • Windows CE operating system
All of the files necessary for a particular firmware release are compressed into a file with a .fup extension.
To determine what is included in any firmware upgrade, see Knowledgebase Document ID: QA1334 - Link to Firmware Maintenance Release information for
PanelView Plus
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal