Select the upgrade type

When you start the Firmware Upgrade Wizard, the first dialog box asks you to select the type of firmware upgrade you want to perform.
To specify the firmware upgrade type
  1. Select
    Upgrade firmware on terminal
    or
    Create firmware upgrade card
    .
  2. If you are creating a firmware upgrade card, specify the card's location and the type of terminal it is for.
  3. Click
    Next
    .
    • If you select
      Upgrade firmware on terminal
      , the next step is specifying a connection.
    • If you select
      Create a firmware upgrade card
      , the next step is specifying the firmware version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal