Select the terminal
If you have a network connection using
FactoryTalk Linx
between the computer and the terminal, select the terminal whose firmware you want to upgrade.To select a terminal
- In theFactoryTalk Linxcommunication tree, click the terminal you want to communicate with.
- ClickNext.
- If you select a valid ME terminal, the next step is to specify a firmware version. Valid terminals includePanelView Plus 7andPanelView Plus 6terminals.
- If you select an invalid ME terminal, an error message shows. Close the message window and select a valid terminal.
Provide Feedback