Select the firmware version for a remote upgrade

After connecting to a valid ME terminal, select the upgrade firmware version.
To select a firmware version
  1. If the location in the
    Firmware source folder
    box is not the folder your firmware source files are stored in, browse for the correct location and specify it in the box.
  2. From the
    Upgrade firmware version
    list, select the firmware version to be used for the upgrade.
    • Click
      Next
      . If your application uses KEPServer OPC servers, the next step is to specify KEPServer drivers.
    • If you have no KEPServer OPC servers, click
      Next
      in the next box to reach the final step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal