Select the firmware version for creating a card

To create a firmware upgrade card, specify the location of the card and select the upgrade firmware version.
To select a firmware version
  1. If the location in the
    Firmware source folder
    box is not the folder your firmware source files are stored in, browse for the correct location and specify it in the box.
  2. From the
    Upgrade firmware version
    list, select the firmware version to be used for the upgrade.
  3. Click
    Next
    .
The next step is to specify KEPServer drivers, if necessary.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal