Complete creating a firmware upgrade card
When you click
Next
in the KEPServer
dialog box, the Firmware Upgrade Wizard shows a summary of the selections you have made during the preceding steps.To complete creating a firmware upgrade card
- If these choices are all correct, clickFinishto complete the process. The Firmware Upgrade Wizard will create a firmware upgrade card, or copy the firmware upgrade source file to the specified folder, from which you can manually copy it to a card.
- If you need to make changes, clickBackto return through the steps and make a different selection.
Provide Feedback