Keyboard shortcuts
You can select menu commands, first press the
Alt
key to make the menu bar active. The shortcut keys are underlined. Press the key corresponding to the menu you want to show. Then use the arrow keys to select the desired item and press Enter
.
TIP:
The shortcuts in this topic are for English versions of Microsoft Operating Systems and may be different for other languages.
The table below is organized by type of task.
Task | Shortcut |
|---|---|
Editing | |
Rename the selection | F2 |
Edit the cell if the selection is in a grid | F2 |
Print | Ctrl+P |
New | Ctrl+N |
Open | Ctrl+0 |
Save | Ctrl+S |
Undo | Ctrl+Z |
Redo | Ctrl+Y |
Cut | Ctrl+X |
Copy | Ctrl+C |
Paste | Ctrl+V |
Find | Ctrl+F |
Asset Find | Ctrl+Shift+F |
Delete | Delete |
FactoryTalk AssetCentre-Specific Functions | |
Toggle Design mode on and off | F3 |
Show Properties of the selected item | F4 |
Navigate & Controlling the Display | |
Refresh | F5 |
Close Asset View | Ctrl+F4 |
Show or switch to Asset View | F7 |
Switch back from the Asset View to the Workspace Pane | Escape |
Hide Asset View (Asset View must be active when using this shortcut) | Alt+W, H |
Move up or down in Asset View (and other functions depending on what control has focus) | Arrow Keys |
Switch between open tabs in the Workspace Pane | Ctrl+Tab |
Move the focus to the next control on the tab or in the dialog box | Tab |
Move the focus to the previous control on the tab or in the dialog box | Shift+Tab |
Click the control with focus. For example, if the OK button in a dialog box has focus, press Enter to in effect, click OK . | Enter |
Dismiss a menu or dialog box without doing anything (like clicking Canel ). | Esc |
Close the active tab in the Workspace Pane | Ctrl+W |
Close FactoryTalk AssetCentre | Alt+F4 |
Online Help | |
Show online help | F1 |
Switch between the help topic and the navigation pane | F6 |
Select a link | Tab |
Open the selected link | Enter |
Show the Options menu (from which you can print) | Alt+O |
Select a book or topic in the Contents | Arrow Keys |
Open the selected book or show the selected topic in the Contents | Enter |
Switch between Contents , Index , and Search tabs in the Navigation pane | Ctrl+Tab |
For more standard Microsoft Windows shortcuts, refer to the online help for your Windows operating system. (Click
Start
, then Help and Support
.)Provide Feedback