Command line parameters for comparison software
The following table describes some of the parameters that may be used. It is not meant to be an exhaustive list.
Parameter | Description |
|---|---|
%Left.Target% | Full path to the first item to compare. Includes the file name when comparing a file. |
%Left.Name% | Name of the first compare item. For a file it is the file name. For a folder it is the last folder name (in alphabetical order). |
%Left.AssetDescription% | Used only if comparing FactoryTalk AssetCentre assets. This is the description (as provided in the asset's properties) for the first asset to compare. |
%Left.AssetPath% | Used only if comparing FactoryTalk AssetCentre assets. This is the full path to the asset in the asset tree, beginning with the top AssetCentre node on the tree. |
%Left.AssetVersion% | Used only if comparing FactoryTalk AssetCentre assets. This is the version number of the first asset to compare. |
%Right.Target% | Full path to the second item to compare. Includes the file name when comparing a file. |
%Right.Name% | Name of the second compare item. For a file it is the file name. For a folder it is the last folder name (in alphabetical order). |
%Right.AssetDescription% | Used only if comparing FactoryTalk AssetCentre assets. This is the description (as provided in the asset's properties) for the second asset to compare. |
%Right.AssetPath% | Used only if comparing FactoryTalk AssetCentre assets. This is the full path to the asset in the asset tree, beginning with the top AssetCentre node on the tree. |
%Right.AssetVersion% | Used only if comparing FactoryTalk AssetCentre assets. This is the version number on the second asset to compare. |
%ReportFilePath% | Full path to save the compare report of Generic FTP or Remote Computer files. |
Provide Feedback