Set asset defaults for schedules

You can set certain default behaviors for scheduled assets, such as email notifications and retries. Default operation properties are set for each type of asset and are applied when an asset is added to a schedule. Changing the default operation settings (and email recipient lists) does not affect assets included in schedules. However, if you modify retry count and interval for a device type, those modifications are applied to assets included in schedules. Retry settings take affect as soon as the schedule is disabled and then re-enabled, or when the schedule is run manually.
Prerequisites
  • To set asset defaults for schedules, you must have
    Edit a schedule
    permission.
To set asset defaults for schedules
  1. Select
    Tools > Options
    .
  2. Under
    Category
    on the left side of the dialog box, select
    Scheduled Operations
    .
  3. Complete the
    Options dialog box: Scheduled Operations
    .
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal