Name Archive Entry dialog box
How do I open the Name Archive Entry dialog box?
- On theSchedulestab, select a Backup and Compare schedule for a device that uses Backup Data, such as a Siemens device or a Generic FTP Device.
- In the lower left portion of theSchedulestab, select the asset.
- In the lower right portion of theSchedulestab, click the browse button in theBackup Compare Partnerbox.
Use the
Name Archive Entry
dialog box, where Name
is the Backup Data binder or file name to specify a version of the Backup Data to compare to files in a backup and compare operation.Provide Feedback