Filename Archive Entry dialog box

How do I open the Filename Archive Entry dialog box?
For a new schedule:
  1. Add a new schedule for a controller (Allen-Bradley Logix 5000, MicroLogix, SLC 500, or PLC-5 controller).
  2. On the third page of the New Schedule Wizard, click in the
    Master File Path Name
    field and click browse_button_small.
For an existing schedule:
  1. Click the
    Schedules
    button to open the
    Schedules
    tab.
  2. Select the Backup or Backup and Compare schedule you want to edit.
  3. In the bottom left, select the controller asset for which you want to select the master file version.
  4. In the bottom right, click in the
    Master File Path Name
    field and click browse_button_small.
Use the
Filename Archive Entry
dialog box to specify which version of the Configuration Data file to use as the master for a Disaster Recovery operation.
Files are kept in Archive where several versions of the same file may be stored. By default, Disaster Recovery operations use the pinned version of the specified file or, if no version has been pinned, the most recent version. Use this dialog box to specify another version for use as the master.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal